2019-09-13 1:11 AM
Hi guys,
I'm working on a new hw design and I can't find the difference between these two references.
Thanks in advance,
Kind regards
2019-09-13 7:38 AM
Hi @Jairo Estefanía , the fundamental difference between the two part numbers is the focus on the temperature sensor of the LIS2DTW12 (T stands for "temperature sensor"). Moreover, the LIS2DTW12 has a lower noise density. These two improvements results in a slightly higher current consumption. Basically the LIS2DTW12 is the upgrade of LIS2DW12, so I suggest you the use of the LIS2DTW12. Regards
2019-09-15 11:19 PM
Thanks @Eleon BORLINI, basically the problem is that there is not enough stock of LIS2DTW12, so we will have to use the LIS2DW12.
2019-09-16 2:12 AM
I understand. How many samples do you need if I can ask? Regards
2019-09-16 2:52 AM
@Eleon BORLINI about 12k
2019-09-16 3:04 AM
Depending on your specific application, I would believe LIS2DW12 should work as well, because the two pn are very similar. Regards
2024-04-11 4:05 AM
Is it true that the LIS2DW12TR has lower noise density than the LIS2DW12 ?
The figures in the datasheets are exactly the same.
2025-06-03 11:51 PM
Hi @Eleon BORLINI ,
Both parts seem to have the temperature sensor and having the same pinpout/configuration.
Can we read the temperature information from LIS2DW12?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.