cancel
Showing results for 
Search instead for 
Did you mean: 

what format is the return buffer of the PDM2PCM function

kcire L.
Associate III

Hello,

I am trying to understand how the PDM_Filter() function works.

If I am using 48Khz with a decimation factor of 64 and a output samples = 16

If I call the function like this...

uint16_t MidBuffer[16];
uint16_t pdmRxBuf[128];

PDM_Filter(&pdmRxBuf[0],&MidBuffer[0], &PDM1_filter_handler);

is the MidBuffer a 16 bit array or a 16 byte array

I am trying to store the PCM data into bytes that I can eventually send out of my UART.

Could anyone please help explain this to me? I have read the app notes and am still confused.

my configuration is below

void MX_PDM2PCM_Init(void)
{
  /* USER CODE BEGIN 2 */
  /* USER CODE END 2 */
 
   /** 
  */
  PDM1_filter_handler.bit_order = PDM_FILTER_BIT_ORDER_MSB;
  PDM1_filter_handler.endianness = PDM_FILTER_ENDIANNESS_BE;
  PDM1_filter_handler.high_pass_tap = 2104533974;
  PDM1_filter_handler.in_ptr_channels = 1;
  PDM1_filter_handler.out_ptr_channels = 1; 
  PDM_Filter_Init(&PDM1_filter_handler);
 
  PDM1_filter_config.decimation_factor = PDM_FILTER_DEC_FACTOR_64;
  PDM1_filter_config.output_samples_number = 16;
  PDM1_filter_config.mic_gain = 0; 
  PDM_Filter_setConfig(&PDM1_filter_handler, &PDM1_filter_config);
 
  /* USER CODE BEGIN 3 */
  /* USER CODE END 3 */
 
}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @kcire L.​ ,

for the PDM_Filter() function description, you can find references in:

But is this post related to this other one?

If so, can you check if that answer can be at least partially valid also for this post?

-Eleon

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.