2020-08-17 1:11 AM
Hi ST engineers,
I would like to figure out how to get accurate measured distance value and getting the value with reasonable interval.
[testing environment]
Nordic NRF52840, vl53l1_platform.c file implemented to use nordic I2C api,
SW version: en.STSW-IMG007 (2.3.3)
refered the reference implementation (STM32CubeExpansion_53L1A1_V2.1.0)
I need only short distance measurement(<1m)
user polling only (not using interrupt)
[VL53L1 test items]
#01. Simple mode
status = VL53L1_WaitDeviceBooted(pdev);
status = VL53L1_DataInit(pdev);
status = VL53L1_StaticInit(pdev);
status = VL53L1_SetDistanceMode(pdev, VL53L1_DISTANCEMODE_LONG);
status = VL53L1_SetMeasurementTimingBudgetMicroSeconds(pdev, 50000);
status = VL53L1_SetInterMeasurementPeriodMilliSeconds(pdev, 500);
status = VL53L1_StartMeasurement(pdev);
RESULT:
There are too many measurement errors(checked via RangingData.RangeStatus that is not 0) and the measured distance is not correct.
#02. fast ranging test
status = VL53L1_WaitDeviceBooted(pdev);
status = VL53L1_DataInit(pdev);
status = VL53L1_StaticInit(pdev);
status = VL53L1_SetPresetMode(pdev, VL53L1_PRESETMODE_LITE_RANGING);
status = VL53L1_SetDistanceMode(pdev, VL53L1_DISTANCEMODE_SHORT);
status = VL53L1_SetMeasurementTimingBudgetMicroSeconds(pdev, 20000);
status = VL53L1_SetInterMeasurementPeriodMilliSeconds(pdev, 25);
status = VL53L1_SetUserROI(pdev, &roiData);
status = VL53L1_StartMeasurement(pdev);
RESULT:
The measured distance roughly correct, but the read interval is too long. it seems to me the value updated interval is longer than 1 sec. I have read the user manual and data sheet. Based on the materials, the fast ranging should be much faster than my test result.
#03. other
status = VL53L1_WaitDeviceBooted(pdev);
status = VL53L1_DataInit(pdev);
status = VL53L1_StaticInit(pdev);
status = VL53L1_SetPresetMode(pdev, VL53L1_PRESETMODE_AUTONOMOUS);
status = VL53L1_SetDistanceMode(pdev, VL53L1_DISTANCEMODE_SHORT);
status = VL53L1_SetMeasurementTimingBudgetMicroSeconds(pdev, 10000);
status = VL53L1_StartMeasurement(pdev);
RESULT:
too many measurement error. update interval is much faster than fast ranging test.
And one more thing I found that is after the FOV change to 4x4 (via VL53L1_SetUserROI) the measured distance looks more accurate.
My Questions are as below.
#A. How can I get correct distance value?
#B. How can I get correct distance value with shorter interval ( ex> 100ms)
I have read the Q&A in ST. But I also have confusion of three mode(VL53L1_PRESETMODE_AUTONOMOUS, VL53L1_PRESETMODE_LITE_RANGING, VL53L1_PRESETMODE_LOWPOWER_AUTONOMOUS)
I don't have experience on ST ToF sensor, so any small help or comment will be much helpful for me.
2020-08-18 3:00 AM
Hi,
The VL53L1_PRESETMODE_LITE_RANGING and VL53L1_PRESETMODE_AUTONOMOUS ranging are not recommended.
Please use only the VL53L1_PRESETMODE_LOWPOWER_AUTONOMOUS.
Accuracy depends on the SNR.
The SNR depends on the return signal rate and the ambient.
The return signal rate depends on the target size, the target reflectance and the distance of the target
Please precise the parameter listed above to help me to help you to improve the measurement accuracy.
Julien
2020-08-19 10:43 PM
Thank you for your reply.
I have folllow up questions.
In my memory, I had tested the VL53L1_PRESETMODE_LOWPOWER_AUTONOMOUS mode. But it was not working. I had got the error at the VL53L1_StartMeasurement.
could you share some code snippet based on that mode?
Thank you in advanced.
2020-08-22 10:08 PM
I have checked ToF custom board with stm32nucleo board with 3.3v. And the sample code that I applied is a AccessRegisters (from en.X-CUBE-53L1A1/STM32CubeExpansion_53L1A1_V2.1.0/Projects/STM32F401RE-Nucleo/Examples/53L1A1/AccessRegisters). And it is working well.
So I'm sure that 3.3v is not a problem although 2.8v is recommended in data sheet.
When I have tested with below setting, there are all of the measurement error..
//Other mode -
status = VL53L1_WaitDeviceBooted(pdev);
status = VL53L1_DataInit(pdev);
status = VL53L1_StaticInit(pdev);
status = VL53L1_SetPresetMode(pdev, VL53L1_PRESETMODE_LOWPOWER_AUTONOMOUS);
// status = VL53L1_SetPresetMode(pdev, VL53L1_PRESETMODE_LITE_RANGING);
status = VL53L1_SetDistanceMode(pdev, VL53L1_DISTANCEMODE_SHORT);
status = VL53L1_SetMeasurementTimingBudgetMicroSeconds(pdev, 20000);
status = VL53L1_SetInterMeasurementPeriodMilliSeconds(pdev, 25);
// status = VL53L1_SetUserROI(pdev, &ur);
// status = VL53L1_SetUserROI(pdev, &roiData);
status = VL53L1_StartMeasurement(pdev);
--------------------------------------------------------------
result
<debug> app: [ToF] 7, 465, 14.85, 4.17
<debug> app: [ToF] 7, 459, 15.10, 4.47
<debug> app: [ToF] 7, 459, 15.10, 4.47
<debug> app: [ToF] 7, 459, 15.10, 4.47
<debug> app: [ToF] 7, 463, 15.14, 4.19
<debug> app: [ToF] 7, 463, 15.14, 4.19
<debug> app: [ToF] 7, 463, 15.14, 4.19
<debug> app: [ToF] 7, 467, 16.20, 4.44
<debug> app: [ToF] 7, 467, 16.20, 4.44
<debug> app: [ToF] 7, 467, 16.20, 4.44
<debug> app: [ToF] 7, 464, 15.01, 4.17
<debug> app: [ToF] 7, 464, 15.01, 4.17
<debug> app: [ToF] 7, 462, 14.96, 4.14
<debug> app: [ToF] 7, 462, 14.96, 4.14
<debug> app: [ToF] 7, 462, 14.96, 4.14
<debug> app: [ToF] 7, 462, 14.87, 4.26
<debug> app: [ToF] 7, 462, 14.87, 4.26
<debug> app: [ToF] 7, 462, 14.87, 4.26
<debug> app: [ToF] 7, 461, 15.21, 4.19
<debug> app: [ToF] 7, 461, 15.21, 4.19
<debug> app: [ToF] 7, 468, 14.56, 4.25
<debug> app: [ToF] 7, 468, 14.56, 4.25
<debug> app: [ToF] 7, 468, 14.56, 4.25
<debug> app: [ToF] 7, 464, 15.16, 4.12
<debug> app: [ToF] 7, 464, 15.16, 4.12
<debug> app: [ToF] 7, 464, 15.16, 4.12
<debug> app: [ToF] 7, 467, 15.60, 4.37
<debug> app: [ToF] 7, 467, 15.60, 4.37
<debug> app: [ToF] 7, 467, 15.60, 4.37
<debug> app: [ToF] 7, 464, 15.53, 4.03
<debug> app: [ToF] 7, 464, 15.53, 4.03
<debug> app: [ToF] 7, 465, 15.10, 4.48
<debug> app: [ToF] 7, 465, 15.10, 4.48
<debug> app: [ToF] 7, 465, 15.10, 4.48
<debug> app: [ToF] 7, 467, 14.13, 4.35
<debug> app: [ToF] 7, 467, 14.13, 4.35
<debug> app: [ToF] 7, 467, 14.13, 4.35
<debug> app: [ToF] 7, 462, 15.70, 4.56
<debug> app: [ToF] 7, 462, 15.70, 4.56
<debug> app: [ToF] 7, 466, 16.06, 4.56
<debug> app: [ToF] 7, 466, 16.06, 4.46
<debug> app: [ToF] 7, 466, 16.06, 4.46
<debug> app: [ToF] 7, 467, 15.71, 4.37
<debug> app: [ToF] 7, 467, 15.71, 4.37
<debug> app: [ToF] 7, 467, 15.71, 4.37
<debug> app: [ToF] 7, 462, 14.61, 4.23
<debug> app: [ToF] 7, 462, 14.61, 4.23
<debug> app: [ToF] 7, 462, 14.61, 4.23
<debug> app: [ToF] 7, 465, 15.61, 4.41
<debug> app: [ToF] 7, 465, 15.61, 4.41
<debug> app: [ToF] 7, 465, 15.80, 4.34
<debug> app: [ToF] 7, 465, 15.80, 4.34
<debug> app: [ToF] 7, 465, 15.80, 4.34
<debug> app: [ToF] 7, 468, 16.01, 4.30
<debug> app: [ToF] 7, 468, 16.01, 4.30
<debug> app: [ToF] 7, 468, 16.01, 4.30
<debug> app: [ToF] 7, 462, 14.12, 4.31
<debug> app: [ToF] 7, 462, 14.12, 4.31
<debug> app: [ToF] 7, 462, 14.12, 4.31
<debug> app: [ToF] 7, 463, 15.47, 4.10
<debug> app: [ToF] 7, 463, 15.47, 4.10
<debug> app: [ToF] 7, 467, 15.04, 4.71
<debug> app: [ToF] 7, 467, 15.04, 4.71
<debug> app: [ToF] 7, 467, 15.04, 4.71
<debug> app: [ToF] 7, 462, 14.94, 4.14
<debug> app: [ToF] 7, 462, 14.94, 4.14
<debug> app: [ToF] 7, 462, 14.94, 4.14
<debug> app: [ToF] 7, 464, 15.77, 4.58
<debug> app: [ToF] 7, 464, 15.77, 4.58
when I tested with below setting
status = VL53L1_WaitDeviceBooted(pdev);
status = VL53L1_DataInit(pdev);
status = VL53L1_StaticInit(pdev);
// status = VL53L1_SetPresetMode(pdev, VL53L1_PRESETMODE_LOWPOWER_AUTONOMOUS);
status = VL53L1_SetPresetMode(pdev, VL53L1_PRESETMODE_LITE_RANGING);
status = VL53L1_SetDistanceMode(pdev, VL53L1_DISTANCEMODE_SHORT);
status = VL53L1_SetMeasurementTimingBudgetMicroSeconds(pdev, 20000);
status = VL53L1_SetInterMeasurementPeriodMilliSeconds(pdev, 25);
status = VL53L1_SetUserROI(pdev, &ur);
// status = VL53L1_SetUserROI(pdev, &roiData);
status = VL53L1_StartMeasurement(pdev);
the result as below with time interval 1~1.5 sec for each line with still much of error..(some are measured )
<debug> app: [ToF] 7, 105, 11.29, 0.00
<debug> app: [ToF] 7, 51, 9.88, 0.00
<debug> app: [ToF] 7, 111, 19.32, 0.01
<debug> app: [ToF] 0, 108, 9.66, 0.01
<debug> app: [ToF] 0, 60, 10.04, 0.00
<debug> app: [ToF] 7, 103, 19.67, 0.03
<debug> app: [ToF] 7, 47, 14.88, 0.01
<debug> app: [ToF] 7, 638, 1.82, 0.09
<debug> app: [ToF] 7, 634, 1.82, 0.09
<debug> app: [ToF] 7, 643, 1.78, 0.08
<debug> app: [ToF] 7, 325, 1.84, 0.09
<debug> app: [ToF] 7, 332, 1.78, 0.09
<debug> app: [ToF] 0, 71, 42.61, 0.01
<debug> app: [ToF] 0, 47, 20.10, 0.00
<debug> app: [ToF] 0, 87, 19.89, 0.00
<debug> app: [ToF] 0, 47, 28.15, 0.00
<debug> app: [ToF] 0, 84, 20.33, 0.00
<debug> app: [ToF] 0, 47, 19.82, 0.00
<debug> app: [ToF] 0, 82, 29.59, 0.00
<debug> app: [ToF] 0, 47, 16.86, 0.00
<debug> app: [ToF] 0, 93, 16.61, 0.00
<debug> app: [ToF] 0, 47, 19.93, 0.00
<debug> app: [ToF] 0, 82, 20.58, 0.00
<debug> app: [ToF] 0, 47, 21.05, 0.00
<debug> app: [ToF] 0, 89, 18.07, 0.00
<debug> app: [ToF] 0, 47, 18.17, 0.00
<debug> app: [ToF] 0, 89, 17.84, 0.00
<debug> app: [ToF] 0, 47, 19.78, 0.00
<debug> app: [ToF] 0, 82, 20.67, 0.00
<debug> app: [ToF] 7, 331, 1.95, 0.07
<debug> app: [ToF] 7, 326, 1.95, 0.08
<debug> app: [ToF] 7, 634, 1.97, 0.07
<debug> app: [ToF] 7, 638, 1.96, 0.07
<debug> app: [ToF] 7, 327, 1.92, 0.07
<debug> app: [ToF] 7, 321, 1.86, 0.07
<debug> app: [ToF] 7, 319, 1.98, 0.07
<debug> app: [ToF] 7, 314, 1.92, 0.07
<debug> app: [ToF] 7, 322, 1.90, 0.08
<debug> app: [ToF] 7, 328, 1.90, 0.07
<debug> app: [ToF] 7, 318, 1.96, 0.07
<debug> app: [ToF] 7, 327, 1.99, 0.06
<debug> app: [ToF] 7, 632, 1.90, 0.07
<debug> app: [ToF] 7, 634, 1.96, 0.06
<debug> app: [ToF] 0, 47, 21.75, 0.01
<debug> app: [ToF] 0, 75, 21.18, 0.00
<debug> app: [ToF] 0, 47, 17.39, 0.00
<debug> app: [ToF] 0, 84, 18.28, 0.00
<debug> app: [ToF] 7, 48, 11.93, 0.00
<debug> app: [ToF] 7, 107, 10.35, 0.01
<debug> app: [ToF] 0, 54, 11.96, 0.00
<debug> app: [ToF] 0, 102, 12.08, 0.00
<debug> app: [ToF] 0, 55, 11.75, 0.00
<debug> app: [ToF] 0, 89, 15.80, 0.00
<debug> app: [ToF] 0, 47, 13.32, 0.00
I think that porting is not a issue due to read device information. Is there a possibility that a porting issue?
My testing environments are as below.
Test env. A: custom ToF board(with 3.3v) with Nucleo board - SUCCESS
Test env. B: custom ToF board with Nordic nrf52840 custom board (with I2C porting) - FAIL
Is there a some HW issue to expect..?? As I checked that 3.3v is not an issue.
( I know this question is very vague that there are so many possibility to figure out issue. )
Any kind of hint or help will be very helpful for me.
Simon
2020-08-23 5:12 AM
Could you share the working code snippet(with parameter setting) for using VL53L1_PRESETMODE_LOWPOWER_AUTONOMOUS ?
BR,
Simon
2020-08-23 5:16 AM
I changed the I2C speed to 100k then it is working. But there is still error on correctness of measurement distance.
if the distance between object and ToF sensor under the 100 mm there is a measurement error about 20mm.
If the distance between object and ToF sensor about 100 mm to 150mm, there is a measurement error about 30mm.
Could someone help me to make it correct measurement?
2020-08-24 8:27 AM
Hi Simon,
You probably need to perform the offset calibration.
Julien
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.