cancel
Showing results for 
Search instead for 
Did you mean: 

Very rarely happens that LSM6DS3 doesn't change state on INT2 pin while new data is available. Is possible that is freezed and only power on reset helps? Config: 0x12, 0x01) 0x12, 0x24) 0x10, 0x48) 0x13, 0x80) 0x11, 0x4C) 0x0D, 0x01) 0x0E, 0x01)

TBurd.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @TBurd.1​ ,

Are you facing the same issue also configuring the INT1 pin instead of the INT2?

Can you also try to latch the interrupt (LIR bit of the TAP_CFG (58h) register)?

You might also compare your code with a C examples on Github like --> lsm6ds3_tap_single.c

-Eleon

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.