2020-09-02 10:15 AM
Hello ST community,
In LIS2DS12 application note, section 5.9.1, it is mentioned that the minimum threshold can be set where 1 LSB = FS/64. I would like to confirm if the value in this register has the unit of g.
Also, if +- 2g is the selected full scale, 1 LSB in STEP_COUNTER_MINTHS is 2/64, right?
Regards,
Anusha
Solved! Go to Solution.
2020-09-03 12:35 AM
Hi @AB.4 , are you referring to the embedded step counter threshold, right? I confirm you the unit is "g", and the STEP_COUNTER_MINTHS (3Ah) is a 6-bit unsigned value, with 1 LSB = 1/64 of FS. To be more specific, this means that in the 2g case the minimum threshold is 2g/64=31.25mg, while in the 4g case is 4g/64=62.5mg.
Please keep in mind that the minimum threshold for step counter recognition is set to a default of 01 0000 in STEP_COUNTER_MINTHS (3Ah) (datasheet p. 57)
As a side note, please consider also that the other threshold definitions are different. For example:
Regards
2020-09-03 12:35 AM
Hi @AB.4 , are you referring to the embedded step counter threshold, right? I confirm you the unit is "g", and the STEP_COUNTER_MINTHS (3Ah) is a 6-bit unsigned value, with 1 LSB = 1/64 of FS. To be more specific, this means that in the 2g case the minimum threshold is 2g/64=31.25mg, while in the 4g case is 4g/64=62.5mg.
Please keep in mind that the minimum threshold for step counter recognition is set to a default of 01 0000 in STEP_COUNTER_MINTHS (3Ah) (datasheet p. 57)
As a side note, please consider also that the other threshold definitions are different. For example:
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.