2019-08-07 3:03 AM
I want to track the swing of cricket-bat using mems sensors. i'm running Motion FX library at 100hz and 200hz. motion fx library is failing some times to track the orientation if the swing speed is more . can I run MotionFx sensorfusion library at 300 hZ? can I use FIFO data and pass more number of input data to compute orientation without increasing the sensorfusion rate?
Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.