cancel
Showing results for 
Search instead for 
Did you mean: 

fp-ind-predmnt1 not connecting to the ST Ble sensor app

reokyouma
Associate III
STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
        Persistent Mode            : Disabled
        Logging Level              : 1
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled
        SWD Debug                  : Enabled
 
Waiting for debugger connection...
Debugger connected
      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.1.0                  
      -------------------------------------------------------------------
 
 
 
Log output file:   C:\Users\reokyouma\AppData\Local\Temp\STM32CubeProgrammer_a06288.log
ST-LINK SN  : 066EFF323338424E43013457
ST-LINK FW  : V2J33M25
Voltage     : 3.26V
SWD freq    : 4000 KHz
Connect mode: Under Reset
Reset mode  : Hardware reset
Device ID   : 0x421
Device name : STM32F446xx
Flash size  : 512 KBytes
Device type : MCU
Device CPU  : Cortex-M4
 
 
 
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a06288.srec
  File          : ST-LINK_GDB_server_a06288.srec
  Size          : 183200 Bytes
  Address       : 0x08004000 
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [1 5]
Download in Progress:
 
 
File download complete
Time elapsed during download operation: 00:00:05.455
 
 
 
Verifying ...
 
 
 
 
Download verified successfully

We have flash the fp-ind-predmnt1 and got this log in STM32CubeIDE which we takes as successful flashing of the firmware but we cannot detect the sensor (STM32F446RE-Nucleo) in our app whether IOS (Iphone 8+ ios 12) or Android (Xiaomi Redmi Note 7 Android 9) in St Ble Sensor app. For the iphone the St Ble sensor cannot connect while in Android it just load a blank page with no info. How can we see the info from the sensor in our app?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
reokyouma
Associate III

inside the firmware is BlueNRG-MS. Just in case it is needed

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.