2024-02-27 7:10 AM
Hello,
I have a requirement to log the data from evaluation board STEVAL-STWINBX1 to cloud. I have created Azure IOT hub and while initiating the cloud logging from the app i was unable to successfully connect to the created IOT Device created in azure even though the connection string was pasted correctly. the application ST BLE Sensor classic automatically disconnects from the sensor once the cloud logging is enabled. do i need to install the SD card and log the data from card to cloud ? I got struck at this point, is there any specific firmware to be loaded, for now I'm just testing with the basic firmware that provides data from all the sensors to the app
2025-11-07 5:21 AM
Hi Dinesh I am also working on a similar project in which i have to condition monitor the wind turbine blade acoustic signals. i would like to know if you have found out the soultion for your problem
kind regards
Jose John
2025-11-07 4:34 PM
Hello Jose,
yes, I was able to connect to the ST cloud but finally settled with Bluetooth communication developing the entire application with Flutter Ble Plus paired with Ble gateway which can push the data back to cloud, let me know if you want to implement something similar.
Regards
Dinesh Kumar
2025-11-10 4:17 AM
Hi Dinesh, Thankyou so much for your reply. i would also like to do the same with WIFI, as the box has a inbuilt WIFI module. As of now would please let me know how did you set up the cloud backup. I really appreciate your help in this as i have not received any reply from community since i posted about this topic. you can also connect to me via LinkedIn (https://www.linkedin.com/in/josejohna).
Kind regards
Jose John
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.