2022-03-17 2:55 AM
Hello Community,
I am working on a machine learning project and I am using an accelerometer sensor "STEVAL-MKI190v1". The board description and documentation can be found on this link The driver files for it is available on this github link. Now I have my example working with a STM Nucleo board with mbed OS on it.
I want to take it further and link it to raspberry pi directly. I want to connect the sensor board directly to raspberry pi and read the accelerometer data via serial port.
My wuestion is is that possible ? If yes how? I went throught web but there are no pythonic support that I found. Has some one tried it? Pleas help!
Thanks
Rick
2022-03-17 3:54 AM
I have not tried this, but there are approaches to address such sensors with Python. A Github project of the similar LIS2DW12 can be found here.
Maybe this helps?
Regards and good luck!
/Peter
2022-03-17 4:27 AM
Thanks for reply @Peter BENSCH . I too cam across this github repository. I am still working on it. It seems to me at this point not very straight forward, but yeah no comments on the solution untill I exhaust my ideas. Lets see what this brings up. Would be great if it actually works. I will share my views in the community after I complete my tries
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.