2024-06-20 4:43 PM
I'm trying to make a demo with the ispu chip ism330is and the STEVAL-MKBOXPRO the issue is I can't find a suitable firmware for the tilebox pro that is compatible with the ispu and allows me upload the compiled UCF program into the chip. Below is a screenshot of the current firmware I'm using FPSNS DATALOG 2 in which it shows the ispu as unknown and if I try to upload the UCF it's just gets stuck!
2024-06-28 12:16 AM
Hi @benx1326 ,
Welcome to ST Community!
Unfortunately ISM330IS firmware for STEVAL-MKBOXPRO is not currently available. We are working on it and it will release in future.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.