2023-11-02 5:04 AM
Hi, I got the reference board of STEVAL-MKI141V2 that has HTS221 temperature and humidity sensor.
#1
I read out the calibration registers by the manual of https://www.st.com/resource/en/technical_note/tn1218-interpreting-humidity-and-temperature-readings-in-the-hts221-digital-humidity-sensor-stmicroelectronics.pdf and the result is following.
H0_rH_X2 (30) = 3A, H1_rH_x2 (31) = 87, T0_degC_x8 (32) = A7, T1_degC_x8 (33) = 16
T2/T0 msb (35) = 4
H0_T0_OUT (36,37) = FFFB, H1_T0_OUT (3A,3B) = D6E4
T0_OUT (3C, 3D) = FFFF, T1_OUT (3E, 3F) = 0310
So the registers value of H0_T0_OUT, H1_T0_OUT also T0_OUT value are minus, is that normal?
#2
It seems the temperature and humidity can be calucuated from there registers. 25.5 degree and 57% RH
but humidity is more 10% higher than other sensors. The accuracy is out of specification value +/- 3.5%.
#3
I want to check the device that using HTS221 sensor, Could you let me know brand and model name if someone knows any products those using HTS221?
Thank you for reading
2023-11-03 8:42 AM
Hi @Take4az ,
Welcome to ST Community!
Have a look at this board Adafruit.
If my reply answered your question, please click on Accept as Solution at the bottom of this post. This will help other users with the same issue to find the answer faster
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.