cancel
Showing results for 
Search instead for 
Did you mean: 

SensorTile.box PRO project in STM32CubeIDE from scratch

stuart_rubin_ns
Associate II

 

Hello. I would like to make a new project for the "SensorTile.box PRO" board using STM32CubeIDE. It appears that the board is not available. (In the image below, you can see that I have filtered on "box" and only the non-pro SensorTile.box device shows up. These two boards are quite different (MCU, peripherals, etc.) so I can't use it.

Is this a bug or omission in the tool? Do I need to add the SensorTile.box PRO BSP manually or something?

Thanks

stuart_rubin_ns_0-1699030180133.png

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.