MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Multiple STHS34PF80 IR sensors nearby each other.

Can several STHS34PF80 IR sensors be used simultaneously, when placed not far from each other, say on the same PCB? If STHS34PF80 infrared sensors are completely passive devices, there should not be any limitations of the distance between them, even ...

aziubin by Associate II
  • 2176 Views
  • 1 replies
  • 1 kudos

Unit of measure for the MEMS IMP23ABSU microphone

Hello, i have searched for this information, but couldnt find it anywhere. Whats the unit of the measured of the MEMS IMP23ABSU mic? I have used the STEVAL-STWINKT1B with the FP-SNS-DATALOG1 from which i created several .csv files that i now need to ...

TomRett by Associate III
  • 12815 Views
  • 14 replies
  • 2 kudos

RMS velocity calculation from accelerometer data

Hello everyone. I'm working on a vibration sensor with RMS velocity output based on measurements from an accelerometer with +-16g maximum acceleration range. There is a simple equation for calculation RMS velocity range and that is : VRMS=Apeak/2*pi*...

MGolm.1 by Associate II
  • 9015 Views
  • 2 replies
  • 0 kudos

LIS2DH12 in molded application

Does anyone know if the LIS2DH12 is ok in a molded application? We have one where we are putting it in a device completely encased in low-pressure molded rubber. The issue we are seeing is that at power up, sometimes the sensor doesn't power up prope...

ande2407 by Associate
  • 1304 Views
  • 1 replies
  • 0 kudos

Horizontal jump measure

I am currently working with a STEVAL-MKI109v3 evaluation card and a STEVAL-MKI217v1 module. I am using UNICO-GUI to collect data from the module, and then processing the data in Python using various filters such as Madgwick, Kalman, and Mahony to enh...

Untitled.png
Isse by Associate
  • 1384 Views
  • 1 replies
  • 0 kudos

Resolved! how it was used as an Accelerometer with FSM

I am using lsm6dso32x.An5629 Datasheet Section 8 FSM Configuration Example implemented only Accelerometer.I don't understand.It seems that you did not set what data(gyro or accel) you use with FSM, but I don't understand how it was used as an Acceler...

sygo by Associate II
  • 1339 Views
  • 1 replies
  • 0 kudos

How to change physical layer of BlueNRG-2?

Hi, We are using STEVAL-STWINKT1B board with a BlueNRG-M2SA BLE module.We want to change the physical layer of the Bluetooth module to utilize bandwidth diversity. But we couldn't figure out how to do this.we have seen "hci_le_set_phy" command in one...

Dogukan by Associate
  • 2764 Views
  • 2 replies
  • 1 kudos

Resolved! LPS22HHTR

Hi, Please provide park date code clarification of "D231". Part Code:LPS22HHTR Thanks, Arun

Arun1_0-1700811475298.jpeg
Arun1 by Associate II
  • 2301 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.