cancel
Showing results for 
Search instead for 
Did you mean: 

Reading SFLP Data from ism330bx

ritzmo93
Associate

I'm trying to extract the data Game Rotation Data from the ism330bx sensor. I'm just not quite sure, which setting to use for that. What I did so far:

Setting the sensor for an ODR of 480Hz with a range of 4000dps and 8g.

(ism330bx_reset(NULL))
(ism330bx_auto_inc(NULL))    // set auto increment register
(ism330bx_set_odr_g(NULL))   // 480Hz
(ism330bx_set_range_g(NULL)) // 8g
(ism330bx_set_odr_xl(NULL))  // 480Hz
(ism330bx_set_range_xl(NULL)) // 8g

 After that I can extract the sensor data from the registers 0x22 to 0x2D.

Now I'm trying to configure the SFLP function in the embedded functions:

  I2C_WRITE_PARAM writeParam = {
                                .Address  = ISM330BX_ADDRESS,
                                .Data     = 0b10000000,     	    
                                .Register = FUNC_CFG_ACCESS
  };  
  i2cWriteSuccess = i2c_write(&writeParam);       // switches to embedded fuunctions

  writeParam.Register = EMB_FUNC_EN_A;
  writeParam.Data     = 0b00000010;
  i2cWriteSuccess = i2c_write(&writeParam);       // activation of SFLP

  writeParam.Register = SFLP_ODR;
  writeParam.Data     = 0b01101011;
  i2cWriteSuccess = i2c_write(&writeParam);       // ODR = 480Hz (for SFLP)

  writeParam.Register = EMB_FUNC_FIFO_EN_A;
  writeParam.Data     = 0b00110010;
  i2cWriteSuccess = i2c_write(&writeParam);       // FIFO Data (GameRotVector, GBIAS, Gravity)

  writeParam.Register = EMB_FUNC_INIT_A;
  writeParam.Data     = 0b00000010;
  i2cWriteSuccess = i2c_write(&writeParam);       // initialisation (für SFLP)

  writeParam.Register = EMB_FUNC_EN_A;
  writeParam.Data     = 0b00000000;
  i2cWriteSuccess = i2c_write(&writeParam);       // switches back from embedded functions

 From what I understand I have to read the SFLP data from the FIFO. However I'm not quite sure how to configure it.

1. Is there a setting (continous FIFO maybe?) to read the SFLP data easily like the sensor data? Which register do I have to use to read the FIFO and how do I know where my SFLP data is located.

2. Is there a mode to read automatically the last data stored. For example I want to do the fusion with a frequeny of 480 Hz, but I would read the data only at 5 to 10 Hz. So I would only be interested in the last calculation of the sensor fusion.

1 REPLY 1
Federica Bossi
ST Employee

Hi @ritzmo93 ,

Have you already tried to look at our examples on Github?

Hope this helps.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.