Resolved! ST BLE sensor APP can't connect
I cannot connect to the ST sensor tile.box when using the ST BLE sensor APP. What should I do?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
I cannot connect to the ST sensor tile.box when using the ST BLE sensor APP. What should I do?
Hello, I'm using STEVAL-MKI109V3 and STEVAL-MKI193V1 (ASM330LHH IMU). Using the Unico GUI, I see that the IMU is detected and recognized however I don't manage to stream any data from the IMU. I enable the accelerometer and the gyroscope and set the ...
Hi, I am looking for an accelerometer. I wonder if there is any ST MEMS chip that meets my requirements:I don't need very high max G force: 4/8G should be enoughLow power consumptionAble to send trigger, like a GPIO rising or falling signal, when acc...
Hello, I am using a LSM6DSL sensor and when applying a 2G acceleration without rotating the board, I get very important spikes on the gyroscopes of about -90°/s to +90°/s amplitude.This is very strange. Is this a normal behaviour from this sensor ? A...
Hi,I have an application with LSM9DS1 sensor and I expected that when I change LSM9DS1 sensor position from horizontal to vertical value will change but changed only when sensor was moving but after that valus comes almost same for horizontal or vert...
In high-accuracy ODR mode, can the frequency of writing to the fifo be automatically aligned,for example 960 to 1000hz
Hi Team,I searched sensor fusion performance information of LSM9DS1TR, LSM6DSO IMUs as below,1. Static Accuracy (Yaw, Pitch, Roll) = ?2. Dynamic Accuracy (Yaw, Pitch, Roll) = ?3. Orientation Settling time = sec?However, I did not find it in the respe...
In MEMS Studio under advanced features > MLC I upload a data pattern and label it under the "Data Pattern" tab. On the "Datalog analysis" tab when I click the Run button it gives the following error.Path: resample_odr.exe does not exist. Please check...
Hello all, I wanted to use sensortile to collect data on microsd card. (I have two of them) So, One portable cradle from the kit working good, but another is not working with the same microsd card. When start it from the android app the sensor just b...
Hello,the LIS2DUX12 documentation (AN5903: LIS2DUX12: machine learning core) contains a table explaining how meta-classifier works:At the third column from the end of the table, the decision tree gives the result "A".As far as I understand, the "B" c...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.