cancel
Showing results for 
Search instead for 
Did you mean: 

Reading data from LSM303AGR

Ester Verlato
Associate
Posted on June 22, 2017 at 15:50

Hi, I'm new here and I am new at working on mems.

I have a LPCXpresso1549 evaluation board and a Steval-MKI172v1 mems that implements a lsm303agr chip. 

I'm working on mbed platform and I need to read values from accelerometer but I tried a lot and cannot read anything.

I connect pins for SCL and SDA, 3V3 to the VDD pin, the GND, and two digital pins to the CS and CS_A (chip select on lsm303agr). 

I don't know what address my lsm303 has and I can't understand what address I need to write on registers

:(

My code is:

&sharpinclude 'mbed.h'

&sharpdefine ACC 0x00

&sharpdefine CTRL_REG1_A 0x20

&sharpdefine CTRL_REG2_A 0x21

&sharpdefine CTRL_REG3_A 0x22

&sharpdefine CTRL_REG4_A 0x23

&sharpdefine CTRL_REG5_A 0x24

&sharpdefine OUT_X_L_A 0x28

&sharpdefine OUT_X_H_A 0x29

&sharpdefine OUT_Y_L_A 0x2A

&sharpdefine OUT_Y_H_A 0x2B

&sharpdefine OUT_Z_L_A 0x2C

&sharpdefine OUT_Z_H_A 0x2D

typedef struct Plane {

      float x, y, z;

} Plane;

Plane a;

//Plane a_max;

//Plane a_min;

Serial pc(USBTX, USBRX); // tx, rx

I2C i2c(P0_23, P0_22);

DigitalOut chip_sel_a(P0_27);

DigitalOut chip_sel_m(P0_28);

void LSM303_write (int data, int reg_address) {

   char out[2] = { reg_address, data };

   i2c.write( ACC, out, 2 );

}

int main() {

//setup iniziale

chip_sel_a = 1;

chip_sel_m = 0;

LSM303_write(0x57, CTRL_REG1_A);

LSM303_write(0x81, CTRL_REG4_A); 

LSM303_write(0x00, CTRL_REG2_A);

LSM303_write(0x00, CTRL_REG3_A);

LSM303_write(0x00, CTRL_REG5_A);

   while(1) {

      char data[1] = { OUT_X_L_A | (1<<7)}; //mette un 1 in testa all'indirizzo per fare read multipla

      char out[6] = {0,0,0,0,0,0};

      i2c.write( ACC, data,1);

      i2c.read( ACC, out, 6);

      a.x = short( (((short)out[1]) << 8) | out[0] );

      a.y = short( (((short)out[3]) << 8) | out[2] );

      a.z = short( (((short)out[5]) << 8) | out[4] );

      pc.printf('asse x: %f\n', a.x);

      pc.printf('asse y: %f\n', a.y);

      pc.printf('asse z: %f\n\n', a.z);

      wait(2);

      }

   }   

Could someone help me?  

:(

#sensor #steval-mki172v1 #lpc1549 #lpcxpresso #mems #lsm303agr
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
S.Ma
Principal
Posted on June 22, 2017 at 19:19

If there is a VDDIO this needs to be the voltage source of the serial interface. 

Read carefully the datasheet and if using the I2C, make sure you can read the WHO_AM_I_REG @0x0F properly for each function (Accelero and Magneto).

Check with an oscilloscope otherwise to make SURE the I2C is looking good and there is a pull-up on each line.

Or sweep all the I2C slave addresses until an ACK is detected...

Miroslav BATEK
ST Employee
Posted on September 04, 2017 at 14:30

If you are using I2C bus, you have to connect pull-up resistors on the SDA nad SCL lines. CS pins needs to be connected to VDDIO. VDDIO also connected to power supply.

The I2C addresses of the sensors are following.

0690X0000060879QAA.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.