2017-06-22 12:56 AM
Hi,
I am planning to use
LSM9DS1
9DoF sensor in our project.As per datasheet table #2, Least significant bit for I2C address is [SDO_ A/G or SDO_M ]= SA0.
From this information & Table#19, I will be able to identify I2C address for
Accelerometer and gyroscope.
How can I set address bit 1 of SAD[1]/SA1 to identify
Magnetic sensor
I2C address?Awaiting for earliest response.
Regards,
Ritesh.
2017-09-04 5:11 AM
Hello Ritesh,
It seems like a typo in the datasheet Table 2 Pin description: SDO_M Pin #6 should set I2C LSB+1 of the device address (SA1) for the magnetometer while LSB (SA0) is always 0. So you can use this pin for your magnetometer identification. I'll ask for datasheet correction.
Regards,
Petr
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.