cancel
Showing results for 
Search instead for 
Did you mean: 

Nice show case! I'm just curious: in a real life scenario, when you really need to be extremely precise in detection, how "far" can you get with this sensor? And in that case what step is the most critical? Data logging? Setting features parameters/filter

Evelina CAMILLERI
ST Employee
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Luca SEGHIZZI
Senior

There are two most critical steps (not only for the real case, but also for the demo): the first one is to get as many relevant data as possible; data logging is therefore the first most critical point. Second, you need to well screen the acquired data and categorize them properly. These steps are fundamental, without a proper logging, data analysis and classification, the final Decision Tree algorithm will perform below the expectations.

View solution in original post

1 REPLY 1
Luca SEGHIZZI
Senior

There are two most critical steps (not only for the real case, but also for the demo): the first one is to get as many relevant data as possible; data logging is therefore the first most critical point. Second, you need to well screen the acquired data and categorize them properly. These steps are fundamental, without a proper logging, data analysis and classification, the final Decision Tree algorithm will perform below the expectations.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.