2019-07-21 3:01 PM
Hey.
I have a small problem with the MPU9250 module, and more specifically AK8963 (Magnetometer). Reading the values measured by the accelerometer and gyro did not cause me major problems and everything works properly. The matter was complicated when I wanted to read the values measured by the magnetometer. In general, communication with the magnetometer works correctly (WHO_AM_I etc.). The problem is that after reading the values from the registers HXL, HXH ... all the time I get the value -1 for each axis.
Code fragment with magnetometer initialization:
MPU9250_Error_code MPU9250_Magnetometer_Configuration(I2C_HandleTypeDef *I2Cx,
struct MPU9250 *DataStructure) {
uint8_t Byte_temp = 0x00;
uint8_t Bytes_temp[3] = {0};
DataStructure->Magnetometer_addres = 0x0C << 1;
// Case 2: Disable the I2C master interface
Byte_temp = 0x00;
if( HAL_I2C_Mem_Write(I2Cx, DataStructure->Device_addres, MPU9250_USER_CTRL, 1, &Byte_temp, 1, 1000) != HAL_OK ) {
//HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
return MPU9250_Magnetometer_Config_FAIL;
}
// Case 3: Enable the bypass multiplexer
Byte_temp = 0x02;
if( HAL_I2C_Mem_Write(I2Cx, DataStructure->Device_addres, MPU9250_INT_PIN_CFG, 1, &Byte_temp, 1, 1000) != HAL_OK ) {
//HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
return MPU9250_Magnetometer_Config_FAIL;
}
// Case 1: Is device connected ?
if( HAL_I2C_IsDeviceReady(I2Cx, DataStructure->Magnetometer_addres, 1, 1000) != HAL_OK ) {
//HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
return MPU9250_Magnetometer_Config_FAIL;
}
// Case 2: Who am i test
if( HAL_I2C_Mem_Read(I2Cx, DataStructure->Magnetometer_addres, MPU9250_WIA, 1, &Byte_temp, 1, 1000) != HAL_OK ) {
//HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
return MPU9250_Init_FAIL;
}
if( Byte_temp != 0x48 ) {
//HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
return MPU9250_Init_FAIL;
}
// Case 4: Setup to fuse ROM access mode and 16-bit output
Byte_temp = 0x1F;
if( HAL_I2C_Mem_Write(I2Cx, DataStructure->Magnetometer_addres, MPU9250_CNTL1, 1, &Byte_temp, 1, 1000) != HAL_OK ) {
//HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
return MPU9250_Magnetometer_Config_FAIL;
}
HAL_Delay(100);
// Case 5: Read from the fuse ROM sensitivity adjustment values
if( HAL_I2C_Mem_Read(I2Cx, DataStructure->Magnetometer_addres, MPU9250_ASAX | 0x80, 1, Bytes_temp, 3, 1000) != HAL_OK ) {
//HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
return MPU9250_Magnetometer_Config_FAIL;
}
DataStructure->Magnetometer_ASAX = ( ( (Bytes_temp[0] - 128) * 0.5 ) / 128 ) + 1;
DataStructure->Magnetometer_ASAY = ( ( (Bytes_temp[1] - 128) * 0.5 ) / 128 ) + 1;
DataStructure->Magnetometer_ASAZ = ( ( (Bytes_temp[2] - 128) * 0.5 ) / 128 ) + 1;
// Case 6: Reset to power down mode
Byte_temp = 0x00;
if( HAL_I2C_Mem_Write(I2Cx, DataStructure->Magnetometer_addres, MPU9250_CNTL1, 1, &Byte_temp, 1, 1000) != HAL_OK ) {
//HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
return MPU9250_Magnetometer_Config_FAIL;
}
// Case 7: Enable continuous mode 2 and 16-bit output
Byte_temp = 0x16;
if( HAL_I2C_Mem_Write(I2Cx, DataStructure->Magnetometer_addres, MPU9250_CNTL1, 1, &Byte_temp, 1, 1000) != HAL_OK ) {
//HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
return MPU9250_Magnetometer_Config_FAIL;
}
HAL_Delay(100);
return MPU9250_Magnetometer_Config_OK;
}Code fragment with reading of measured values:
MPU9250_Error_code MPU9250_Read_Magnetometer(I2C_HandleTypeDef *I2Cx,
struct MPU9250 *DataStructure) {
uint8_t Bytes_temp[7] = { 0x00 };
if( HAL_I2C_Mem_Read(I2Cx, DataStructure->Magnetometer_addres, MPU9250_HXL | 0x80, 1, Bytes_temp, 7, 1000) != HAL_OK ) {
//HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
return MPU9250_Read_Magnetometer_FAIL;
}
DataStructure->Magnetometer_X = Bytes_temp[0] | Bytes_temp[1] << 8;
DataStructure->Magnetometer_Y = Bytes_temp[2] | Bytes_temp[3] << 8;
DataStructure->Magnetometer_Z = Bytes_temp[4] | Bytes_temp[5] << 8;
return MPU9250_Read_Magnetometer_OK;
}
2019-07-22 3:19 AM
Hi @MNowa.10 , MPU9250 module is a TDK and not an ST module :smiling_face_with_smiling_eyes: These libraries (HAL_I2C_Mem package) are intended to work for ST sensors (e.g. LSM9DS1 i-Nemo module). I suggest you to share your question with TDK and STM32 community; in case you are interfacing the module with an Arduino, I suggest you to directly post your question to TDK support. Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.