2021-02-18 9:18 AM
Hi,
I'm testing the MotionFX library with the Discovery Kit IoT node [B-L4S5I-IOT01-A] and I have a problem: randomly the sensor fusion algorithm "explodes" and I can only get only "nan" values for all the `MFX_MagCal_output_t` values, Gyro Biases included.
What can be the cause of this behavior?
Following my initialization code:
int32_t initMotionFX()
{
char lib_version[MFX_STR_LENG];
MFX_knobs_t iKnobs;
/* Sensor Fusion API initialization function */
MotionFX_initialize();
MotionFX_GetLibVersion(lib_version);
MotionFX_getKnobs(&iKnobs);
iKnobs.LMode = 1;
iKnobs.gyro_orientation[0] = 'n';
iKnobs.gyro_orientation[1] = 'w';
iKnobs.gyro_orientation[2] = 'u';
iKnobs.acc_orientation[0] = 'n';
iKnobs.acc_orientation[1] = 'w';
iKnobs.acc_orientation[2] = 'u';
// Note: the magnetometer is rotated by 180° respect to the IMU
iKnobs.mag_orientation[0] = 's';
iKnobs.mag_orientation[1] = 'e';
iKnobs.mag_orientation[2] = 'u';
MotionFX_setKnobs(&iKnobs);
// ----> Experimental init bias value
// Note: to be replaced by flash memory reading
init_gyro_calib[0] = 0.08;
init_gyro_calib[1] = 0.02;
init_gyro_calib[2] = 1.02;
MotionFX_setGbias(init_gyro_calib);
// <---- Experimental init bias value
MotionFX_enable_6X(MFX_ENGINE_ENABLE);
MotionFX_enable_9X(MFX_ENGINE_ENABLE);
return 0;
}
Solved! Go to Solution.
2021-02-26 5:51 AM
Thank you for checking the code.
I have a log application that I can use to save the data. I only need to modify it to retrieve also the mag raw and biases.
I will share the data as soon as they are ready
2021-02-26 7:03 AM
@Miroslav BATEK you can download the log here in CSV format: https://www.dropbox.com/s/e5mvywc2evehkxr/20210226_155357-SensorsDataCompare.zip?dl=0
The columns `MFX_MAG_CALIB_IN_TS`, `MFX_MAG_CALIB_IN_X`, `MFX_MAG_CALIB_IN_Y`, `MFX_MAG_CALIB_IN_Z`, `MFX_MAG_CALIB_OUT_X`, `MFX_MAG_CALIB_OUT_Y`, `MFX_MAG_CALIB_OUT_Z` contain the data exactly as they are used in the firmware, without any kind of conversion:
TS in msec
MFX_MAG_CALIB_IN in µT/50
MFX_MAG_CALIB_OUT in µT/50
2021-02-26 1:02 PM
@Miroslav BATEK Thank you for your support. I finally found the issue. The "nan" problem was generated by the "timestamp overflow".
In the IMU Task, I have a code that handles the overflow and recast the timestamp on a `uint64_t` variable, but there was a wrong comparison between "raw" timestamp and "timestamp*25".
I fixed it and I left the board running for more than 9 hours without any issue.
Thank you very much
Walter
2021-02-28 11:54 PM
I'm glad you have found the issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.