MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SM32Cube IDE MEMS1

Hello ST MEMS Community.I recently switched to use STM32 CubeMX IDE and I really like it .I would to utilize full power of the IDE and would like to use MEMS sensor for my application. I have installed X-CUBE MEMS pack.I did see multiple device avai...

IB.1 by Associate III
  • 2808 Views
  • 5 replies
  • 0 kudos

Resolved! Data corruption with PDM Microphone

Hello, I am using a MEMS PDM microphone and reading it in using I2S. The following parameters are set in my I2S and PDM configurations.hi2s3.Instance = SPI3; hi2s3.Init.Mode = I2S_MODE_MASTER_RX; hi2s3.Init.Standard = I2S_STANDARD_MSB; hi2s3.I...

kcire L. by Associate III
  • 5282 Views
  • 11 replies
  • 0 kudos

How do you calculate the tri-axis(mag, access, gyro or fusion) outputs (+/- 1over 180 degrees) to accurately cover 360 degrees in code and what are those conversion. So that one physical rotation of the device equals 360 degrees exactly.

How do you calculate the tri-axis(mag, access, gyro or fusion) outputs (+/- 1over 180 degrees) to accurately cover 360 degrees in code and what are those conversion. So that one physical rotation of the device equals 360 degrees exactly. Currently us...

CTone.1 by Associate
  • 1469 Views
  • 1 replies
  • 0 kudos

[Webinar] Would you like to learn more about Content Level Management Applications using ST FlightSense Time-of-Flight Sensors?

Join our 1-hour webinar to discover how ST Time-of-Flight proximity and ranging sensors can beat content level monitoring challenges Tuesday, March 2nd, 2021 | 3:00 pm CETYou will learn:The benefits ToF sensors in content level management application...

0693W000007ZigEQAS.png

Resolved! MotionFX "nan" values after a while on Discovery kit IoT node

Hi,I'm testing the MotionFX library with the Discovery Kit IoT node [B-L4S5I-IOT01-A] and I have a problem: randomly the sensor fusion algorithm "explodes" and I can only get only "nan" values for all the `MFX_MagCal_output_t` values, Gyro Biases inc...

Resolved! Fluctuation of gyro angular velocity data of LSM6DSL motion sensor

First of all, I apologize for my unprofessional English!In the process of using STM32 board to collect data from lsm6dsl module, the angular velocity data of gyroscope can be output stably, but there are jumps in the angular velocity of three directi...

0693W000007ZJUXQA4.png 0693W000007ZJUwQAO.png 0693W000007ZJVBQA4.png 0693W000007ZJVGQA4.png
BWu.4 by Associate II
  • 2648 Views
  • 4 replies
  • 1 kudos

Resolved! Doubt 6D orientation mode(LIS2DW12)

Hi,I am using an accelerometer (LIS2DW12) from STMicroelectronics. An interrupt is generated only for (50,60,70,80) degrees only while setting on 6D orientation mode. I would expect to get an interrupt for even small degrees of tilt starting from 10 ...

MIR.1 by Associate II
  • 3010 Views
  • 5 replies
  • 0 kudos

Outliers after moving average processing

Hello community,in my current project I use a NUCLEO-H743ZI2 to acquireaccelerations and angular velocities from a LSM9DS1 (high and low byte - let's call it raw data). The serial transmission to my computer works well.Due to errors in acquired value...

CKolh.1 by Associate
  • 2007 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.