2019-05-03 2:37 AM
Hi,
I'm trying to implement the streaming of two MEMS microphones via I2S.
Following some examples provided by ST, I was able to implement the acquisition of the two microphones: I obtain a 32 samples buffer PCM every 1 ms (left and right channel).
Now I'm trying to send these samples through I2S (16 Bits Data on 16 Bits Frame, 16 KHz) using DMA in circular mode. So, I can fill the buffer while the transmission goes on.
I've created a 128-elements buffer. Every 1 ms I put in the buffer 32 elements. When the buffer contains 64 elements, I launch the transfer using "HAL_I2S_Transmit_DMA".
The problem is that probably the DMA transfer goes slowly compared to the 1 ms filling routine, so what I obtain is that the sound isn't clear.
How can I sync these two operations?
Solved! Go to Solution.
2019-05-07 7:13 AM
Hi Fib, could you share some more details of your code? The procedure you are doing is similar the kind of processing of the Bluecoin tool (https://www.st.com/content/st_com/en/products/embedded-software/evaluation-tool-software/stsw-bcnkt01.html:( here there is an example called Audio Loopback that exactly performs what you are wishing to do. Regards
2019-05-07 7:13 AM
Hi Fib, could you share some more details of your code? The procedure you are doing is similar the kind of processing of the Bluecoin tool (https://www.st.com/content/st_com/en/products/embedded-software/evaluation-tool-software/stsw-bcnkt01.html:( here there is an example called Audio Loopback that exactly performs what you are wishing to do. Regards
2019-07-29 12:29 AM
Hello. I have the same problem.
Have you solved your problem ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.