2024-07-02 11:37 AM - last edited on 2026-03-16 8:25 AM by Andrew Neil
I have an X-NUCLEO-IKS4A1 mounted on top of a NUCLEO-L476RG and I am trying to connect that to Mems Studio. I get one of the two errors in the attached screenshots. Either "Board not identified" or "Some device is already connected".
2026-03-19 8:43 AM
Hello @Apollo1
We are checking the generated code for NUCLEO-H503RB and will get back to you shortly.
2026-03-20 8:23 AM
Hello @Apollo1
My colleague analyzed the project and here are his recommendations:
2026-03-23 1:10 PM - edited 2026-03-23 1:35 PM
Hi Miroslav,
I was able to generate the code, build and program the board using the H503RB_MEMS_App_ST.ioc file you provided. MEMS-Studio was able to connect to the board successfully.
I have tried updating my version of the ioc file in Cube-MX and I wanted to add some comments based on your feedback and point to some issues I experienced in the process.
- I've changed TIM1 to TIM3.
TIM1 does work, however, I think TIM1 should be allocated for more complex setup such as Half-H bridge implementation (BLDC or Digital Power Supply).
TIM3 is a basic general purpose timer.
- I've changed USART2 to USART3.
On MB1814 project schematic for NUCLEO-503RB, UART over USB (Virtual Com Port) signals VCP_RX and VCP_TX are mapped to pin PA3 and PA4 which belong to USART3.
Within Cube-MX, pin assignment for signals VCP_RX and VCP_TX can be found under "Bsp" section when "Human Machine Interface" with VCOM is checked. Though VCOM has to remain "Unchecked" as it can't be used in the X-CUBE-MEMS1 USART "Found Solutions".
- I've increased Minimum Stack Size to 0x4000.
Using default "Minimum Stack Size" of 0x400 will cause a HardFault.
The HardFault condition can only be seen when running STM32Cube_IDE in debug mode.
So best to avoid using MEMS-Studio "Firmware Programming" to flash the board until it has been shown that MEMS-Studio has been able to connect.
- Circular Mode in DMA settings has to be disabled.
- Now the project generates correctly and works with MEMS Studio, you can try the attached ioc.
- You can find settings description for devices supporting Linked-List in chapter 4.3.2 of User Manual for X-CUBE-MEMS1 v12.0.0. We do not set LINKEDLIST section in CubeMX for our projects, you can compare your project to "X-CUBE-MEMS1_v12.0.0"\Firmware\Projects\NUCLEO-U575ZI-Q\Applications\IKS4A1\DataLogFusion\ for details.
I did follow up on the documentation but I may have overlooked or misinterpreted the "Circular Mode" setting.
Having "Circular Mode" set to "Enable" will cause the following error during the build:
error: 'NodeConfig' undeclared (first use in this function)
666 | NodeConfig.NodeType = DMA_GPDMA_LINEAR_NODE;
| ^~~~~~~~~~
On a side note, if "Visibility (Static)" for the Timer is "checked" (under "Project Manager" => "Advanced Settings"), the following error will be reported:
undefined reference to `MX_TIM3_Init'Once all the above steps have been taken care of, then I can successfully build the code and connect with MEMS_Studio.
PS. In STM32Cube_IDE, the build will fail with the default project settings returning the following error:
../arm-none-eabi/bin/ld.exe: H503RB_MEMS_App.elf section `.text' will not fit in region `FLASH'
../arm-none-eabi/bin/ld.exe: region `FLASH' overflowed by 5880 bytesChanging the project "Optimization level" to "Optimize for size ..." does fix the issue.
When using a NUCLEO MCU board, the add-on sensor expension board (ie. IKS4A1) isn't required to successfully establish a connection. Though trying to acquired sensor data will fail.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.