2024-02-15 1:07 AM
Is it possible to execute features such as pedometer, activity/inactivity detection, tilt/tap, with same configuration of ODR, Full scale? How can I include all these features in a single program?
Can someone explain this please
Solved! Go to Solution.
2024-03-01 3:00 AM
Hi @Varsha ,
You can set the same ODR for both (e.g. 833Hz) because then the pedometer internally always runs at 26Hz anyway, so it is not impacted by the ODR you set.
2024-02-15 2:29 AM
Hi @Varsha ,
Yes, you can. You can find some examples on the AN5272 for each embedded function.
Please note that for the tap detection we suggest to use an high ODR (e.g., 416 Hz or 833 Hz), the pedometer and tilt always works at 26Hz internally.
For the FS we suggest you 8g or 16g.
2024-02-15 3:57 AM
@Federica Bossi Thank you.
Suppose if I want to configure both pedometer and tap detection feature in a single program/file, how do I select the acc and gyro ODR, since both features run on different ODR
2024-03-01 3:00 AM
Hi @Varsha ,
You can set the same ODR for both (e.g. 833Hz) because then the pedometer internally always runs at 26Hz anyway, so it is not impacted by the ODR you set.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.