2019-06-13 6:05 AM
Hi,
How can I get the linear acceleration from a LSM6DSO? Is there any filter that I can apply?
Regards,
Gabriel
2019-06-14 4:01 AM
Hi Gabriel, you can apply an embedded LP filter acting on LPF2_XL_EN in reg CTRL1_XL (10h). Consider also that you can set ODR 1.6Hz (12.5Hz in HP mode) do have only (anti-alias filter will cut the frequencies higher than ODR/2). Btw, please note that in the Low pass filer case you have to take into account the settling time of the filter itself, that can be regulated acting on FASTSETTL_MODE_XL of register CTRL8_XL (17h). Consider that due to the earth gravity you'll always have 1g modules acceleration distributed on the 3 axis. To handle this vale you should subtract it in post-processing. Regards
2019-06-20 1:08 AM
Hi Eleon,
I will test it and give you some feedback.
Thanks,
Gabriel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.