cancel
Showing results for 
Search instead for 
Did you mean: 

Lsm6dso : how to get accelerometer data in FIFO

ADvor.2
Associate II

I'm working with lsm6dso for activity monitoring project. I want to record the acc and gyro data in the fifo and trigger an interrupt when the number of samples in fifo are more than the configured watermark. I already achieved to get the gyro data in the fifo and trigger the interrupt when the number of samples equals the watermark.

My problem is that I only get gyroscope data and no acc data. Do I have to write to a special register in order to enable the acc? I apreciate any help regarding the topic how to get acc running in fifo mode.

Best regards ​

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Eleon BORLINI
ST Employee

Hi @ADvor.2​ ,

did you correctly configured both the ODRs of the axl and the gyro?

You might also compare your code with the example on Github --> lsm6dso_fifo.c

-Eleon

SS13
Associate II

Another thing to check is that the Batching Data Rate in FIFO_CTRL3 is set for XL.

Yes, I already checked the fifo example in fifo. The code I'm using is based on it and the register are setted as in the example

Setting or not setting the batching data rate in fifo_ctr3 didnt affect at all.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.