2024-04-29 1:57 AM
Hi,
I am trying to configure interrupt on LSM6DSLTR module but I am not able to get any interrupt on the pin INT1.
I am using nrf52 dk for setting interrupt on pin.
err_code = nrf_drv_mpu_write_single_register(LSM6DSL_ACC_GYRO_INT1_CTRL, 0x03);
if(err_code != NRF_SUCCESS) return err_code;
err_code = nrf_drv_mpu_write_single_register(LSM6DSL_ACC_GYRO_TAP_CFG1, 0x90);
if(err_code != NRF_SUCCESS) return err_code;
err_code = nrf_drv_mpu_write_single_register(LSM6DSL_ACC_GYRO_WAKE_UP_DUR, 0x00);
if(err_code != NRF_SUCCESS) return err_code;
err_code = nrf_drv_mpu_write_single_register(LSM6DSL_ACC_GYRO_WAKE_UP_THS, 0x02);
if(err_code != NRF_SUCCESS) return err_code;
err_code = nrf_drv_mpu_write_single_register(LSM6DSL_ACC_GYRO_MD1_CFG, 0x20);
if(err_code != NRF_SUCCESS) return err_code;
After configuring interrupt my values becomes repeated or same
<info> app: 251781.25, 231621.25, 231621.25, 1755.82, 1755.82, 1755.82
<info> app: 33643.75, 13483.75, 13483.75, 235.09, 235.09, 235.09
Can you please guide me, if what I am doing is right or not ? If its not right please let me know how can i configure the interrupt properly.
2024-04-29 3:40 AM
WAKE_UP_THS, How to do this calculation?
2024-04-30 2:25 AM
@Federica Bossi, If you could help me. I have got interrupt on the INT1 pin but it is consuming power. How can i reduce the power consumption. from mA to uA. What settings should I apply?
2024-04-30 2:49 AM
Hi @yash2530 ,
You can try implementing our PID example on github. It is developed in the best condition to have the lowest consumption.
Above all, I advise you not to turn on the gyroscope if you want to reduce power consumption since you don't need it for wake up.
2024-05-03 10:28 PM
@Federica Bossi Can you also guide on how I can generate an interrupt based on angle of rotation? Is it possible?
I have a use case what I want to detect if the mem sensor is rotated suppose 15 degree then only it starts throwing values.
If this is not possible, then is there any way I can achieve a motion threshold higher, And how is the wake up threshold calculated.
Thanks
2024-05-20 3:48 AM
@Federica Bossi waiting for your reply!!
2024-05-30 5:19 AM
Hi @yash2530 ,
We don't have any examples for this specific case but you can try different threshold values in terms of amplitude and duration and see if something changes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.