2019-02-11 4:19 AM
Hello,
I'm planning on using the LSM6DSL in my design.
For the same reason I have bought & worked on evaluation board, STEVAL-MKI178V1 .
In the documentation of this board, I have found that pin no. 10 & pin no. 11 both are used & connected.
But in LSM6DSL datasheet these pins are shown as NC pins.
I'm getting the data using evaluation board, but unable to get the data using IC only.
I'm using nordic processor & through I2C communication I'm reading the accelerometer & gyro values.
Do I need to connect pin no. 10 & 11 in hardware?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.