cancel
Showing results for 
Search instead for 
Did you mean: 

lsm6ds3trc free fall detect

Jali
Associate II

Dear,

I'm testing the lsm6ds3tr-c free fall function, but it's hard to tuning the threshold, i attach the current registor settings, I want to dectect the 1m free fall, can you give some guide? thanks a lot.

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Jali ,

Have you already tried to implement the simple example on the AN?

1. Write 60h to CTRL1_XL // Turn on the accelerometer
// ODR_XL = 416 Hz, FS_XL = ±2 g
2. Write 81h to TAP_CFG // Enable interrupts and latch interrupt
3. Write 00h to WAKE_UP_DUR // Set event duration (FF_DUR5 bit)
4. Write 33h to FREE_FALL // Set FF threshold (FF_THS[2:0] = 011b)
// Set six samples event duration (FF_DUR[5:0] = 000110b)
5. Write 10h to MD1_CFG // FF interrupt driven to INT1 pin

 

The INT1_INACT_STATE is needed for activity/inactivity detection.

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Jali
Associate II

if I need enable the INT1_INACT_ STATE of MD1_CFG(5Eh)?

Hi @Jali ,

Have you already tried to implement the simple example on the AN?

1. Write 60h to CTRL1_XL // Turn on the accelerometer
// ODR_XL = 416 Hz, FS_XL = ±2 g
2. Write 81h to TAP_CFG // Enable interrupts and latch interrupt
3. Write 00h to WAKE_UP_DUR // Set event duration (FF_DUR5 bit)
4. Write 33h to FREE_FALL // Set FF threshold (FF_THS[2:0] = 011b)
// Set six samples event duration (FF_DUR[5:0] = 000110b)
5. Write 10h to MD1_CFG // FF interrupt driven to INT1 pin

 

The INT1_INACT_STATE is needed for activity/inactivity detection.

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.