cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DW12 Activity and Free Fall Detection

ABane.1
Associate III

Can someone help me how to use one interrupt pin for Activity/Inactivity and another for Free Fall detection? I need to use it in the lowest possible possible mode as my device is coin cell battery powered.

Regards,

Asish Banerjee

2 REPLIES 2
Federica Bossi
ST Employee

Hi @ABane.1 ,

Have you already looked at our official examples on Github?

Let me know if this helps :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hello @Federica Bossi ,

I have already checked the examples in Github. In the activity and free fall examples, INT1 pin is used for both detection. Where as I am now following the following Youtube video by ST for activity/Inactivity detection and it is working as desired but current consumption is higher than the presentation showed. (1.3uA in inactive mode and around 6-7uA in active mode. Current measured with two 10k pull up resistor for SCL & SDA lines.)

https://www.youtube.com/watch?v=HgPVZLw6zeI

Now if I increase ODR to 200Hz according to free fall detection example, active current will be again higher. Can you please suggest me how to use both detection provided I can keep the power consumption as minimum possible. 

Regards,

Asish Banerjee

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.