2021-09-01 3:43 PM
Hello,
I am using the FIFO to read the gyroscope and accelerometer data from the LSM6DS33 using a Raspberry Pi. It is connected over I2C at a frequency of 400kHz. Currently it takes between 4-7 seconds of constant reading to empty out the FIFO and by then it's almost full again. Is there a way to do a bulk read of the FIFO rather than read each sensor reading separately?
Thanks,
Mahmoud
Solved! Go to Solution.
2021-09-03 5:37 AM
Hi, if you configure the LSM6DS33 in FIFO mode (i.e. the filling of the FIFO stops when the limit is reached), and you choose the ODR, it will take 1/ODR * FIFO size (8 kbyte) to fill the FIFO. You have to configure the FIFO_CTRL5 (0Ah) register, in FIFO mode, and you can program a custom FIFO threshold in FIFO_CTRL1 (06h) and FIFO_CTRL2 (07h).
2021-09-03 5:37 AM
Hi, if you configure the LSM6DS33 in FIFO mode (i.e. the filling of the FIFO stops when the limit is reached), and you choose the ODR, it will take 1/ODR * FIFO size (8 kbyte) to fill the FIFO. You have to configure the FIFO_CTRL5 (0Ah) register, in FIFO mode, and you can program a custom FIFO threshold in FIFO_CTRL1 (06h) and FIFO_CTRL2 (07h).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.