2017-04-05 2:44 AM
I have an LSM6DS3 gyro / accelerometer connected to a Raspberry Pi 3B using i�c. I'm using the internal FIFO to get samples from the gyro and accelerometer. The data is plausible most of the time, however, every now and then there is a strange sequence of values when I read the FIFO:
sample output:
47 -240 -371 143 -238 -378 ...
138 -240 -369 141 -238 -361 ...137 -238 -381 134 -247 -373 ...130 -229 -367 133 -235 -370 ...134 -236 -364 127 -241 -371 ...2609 -155 453
1110 1497 2450 -73 160 499 7588 6995 16508 15758 10954 28583 11959 7888 20306 10 508 64 9 -56 -411 117 -190 -295 142 -250 -271 ...133 -232 -408 133 -235 -319 ...136 -240 -388 129 -238 -361 ... 142 -240 -378 143 -240 -354 ...139 -238 -375 137 -244 -374 ...so there is one readout without any samples, followed by three readouts with implausible data.
This behaviour always occurs for the first readout when I connect, then afterwards it occurs sporadically.
Can you tell me where this could come from?
thanks, best regards
Christian
#lsm6ds3 #sensor #accelerometer2017-04-05 7:36 AM
Hello,
You can try following recommendations:
I hope it helps.
Best regards,
PetrWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.