2025-03-25 5:40 PM
Anyone have any idea if the temperature can remain the same for long periods of time in a stable environment?
2025-03-27 7:25 AM
Hi @hmckee ,
It should. Did you try?
2025-03-27 2:23 PM
Yes, that's the issue. We've set up our device so that it marks the LPS22 in error if it reads the same value 45 times in a 30 min period. The condition has occurred in both a stable, temperature controlled environment and in an uncontrolled environment.
The purpose of this was to determine if the LPS22 is functioning properly. Maybe this is an unrealistic expectation.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.