2020-03-04 7:32 AM
Hello,
I have a LIS2DS12 accelerometer connected to an arduino MKR1000 through SPI.
For my application I need to use the highest ODR of 6400 Hz, and 2g FS.
In order to collect 1 s of acceleration data, I constantly pull data from the FIFO. I set the threshold to 5, and FIFO in continuous mode.
In the attached plot, you see X, Y and Z acceleration data with LIS2DS12 standing still on my table, with a very high noise!
In order to understand the origin of such a high noise, I first get a full FIFO and then I start to pull out data through SPI.
In such a way you can see that first 256 values have a certain noise, while as soon as I start SPI communication the noise increases.
Is this a knows issue?
Thanks a lot.
2020-03-06 5:12 AM
Hi @Avian.1 , so you are basically filling the FIFO up to 5 samples (at ODR 6400Hz, threshold = 5), and then you read the FIFO content via SPI, right?
If you set a threshold, you should work in pure FIFO mode, i.e. stops collecting data when FIFO is full. As noted in the AN4748 p 43:
Follow these steps for FIFO Continuous configuration which sets a threshold to generate an interrupt to trigger a read by the application processor:
1. Set FTH[7:0] to 255.
2. Set INT2_FTH to ‘1’: Enable FIFO threshold interrupt
3. Activate Continuous mode by setting the FMODE[2:0] field to 110b in the FIFO_CTRL register (25h).
Regards
2021-12-01 6:02 AM
Hi @Avian.1 (Community Member)
I have a same problem like you.
If you have solved this problem, please let me know how you solved it.
Thank you
-Yonghun
2021-12-01 6:19 AM
Hi Yonghun,
I'm sorry to tell you that I've tried a lot changing fifo mode, setting interrupts, and so but noise was always there.
At the end, I gave up and changed accelerometer (IIS3DWB).
I just think that LIS2DS12 is not made to work at high ODR.
2021-12-01 6:25 AM
Hi @Avian.1 (Community Member)
thank you for helping me.
Do you know a site where I can get IIS3DWB??
I am currently struggling with the lack of stock for that sensor.
I mainly use Digi-Key and Mouser sites.
Thank you
-Yonghun
2021-12-01 8:14 AM
Hi @YSong.3 ,
some products are still out of stock in this period, but things are recovering.
Especially in case you need more than 500 samples, I suggest you to directly check the ST eStore and to Contact Sales as indicated in the last row.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.