cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DS12 读�?�传感器温度一直�?�?�?�?�

1123.3
Associate

值一直是0x80 用热风枪和制冷风扇�?�过都�?�?�​

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @1123.3​ ,

Is this translation correct?

LIS2DS12 reads the sensor temperature and keeps the same.

The value is always 0x80. It will not change if you blow it through with a heat gun and cooling fan​.

If so, did you configured the FS and the ODR, before starting the readout of the temperature sensor?

Note that it's ODR is 12.5Hz., so if you are running the sensor with higher ODR, polling the output registers you might read several time the same temperature value.

 /* Enable Block Data Update. */
  lis2ds12_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
  /* Set full scale. */
  lis2ds12_xl_full_scale_set(&dev_ctx, LIS2DS12_2g);
  /* Set Output Data Rate. */
  lis2ds12_xl_data_rate_set(&dev_ctx, LIS2DS12_XL_ODR_100Hz_LP);

-Eleon

View solution in original post

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @1123.3​ ,

Is this translation correct?

LIS2DS12 reads the sensor temperature and keeps the same.

The value is always 0x80. It will not change if you blow it through with a heat gun and cooling fan​.

If so, did you configured the FS and the ODR, before starting the readout of the temperature sensor?

Note that it's ODR is 12.5Hz., so if you are running the sensor with higher ODR, polling the output registers you might read several time the same temperature value.

 /* Enable Block Data Update. */
  lis2ds12_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
  /* Set full scale. */
  lis2ds12_xl_full_scale_set(&dev_ctx, LIS2DS12_2g);
  /* Set Output Data Rate. */
  lis2ds12_xl_data_rate_set(&dev_ctx, LIS2DS12_XL_ODR_100Hz_LP);

-Eleon

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.