cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DH12: Measures higher accelerations than maximum range of 16 g

Philipp D
Associate II

Posted on April 05, 2018 at 02:02

I'm currently testing the LIS2DH12 for a project concerning shock detection and measurement.

My first question is:

Which scaling factor do I have to use at the threshold registers and which one at the readout values for +- 16 g, Low Power mode (LP). Do I get this right that they are different?

Readout values: 192 mg / LSB

Threshold registers (INT1_THS, INT2_THS): 186 mg / LSB

My next question is about the maximum valid range

I tested the maximum readout values at +-16 g in low power mode at 5376 Hz.

Inside the OUT register I do have 8 bit-values of +127 or -128 at one or two out of the 3 axis.

That would mean: 127 x 0.192 g = 24.384 g

Is this value still correct because it's a bit more than 10 % above the maximum range of +- 16g?

Many thanks in advance for your help!

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Not applicable
Posted on April 05, 2018 at 15:48

Hello,

Have a look at this answer to one of my previous question (it is related to a magnetometer, but the principle is the same).

https://community.st.com/0D50X00009XkXwiSAF

Long story short: boundaries are guaranteed as stated in the datasheet, the values outside the boundaries are not guaranteed to be meaningful.

David

Miroslav BATEK
ST Employee
Posted on April 05, 2018 at 16:55

The functionality above the 16g is not guaranteed.

The output can be not linear and can vary piece by piece

Posted on April 05, 2018 at 16:12

Hi David, 

Many thanks for your reply!

Are you directly from the ST Support Team? I just wanted to know if this Info is officially valid because I want to use the solution in production Code.

Best regards 

Philipp 

Not applicable
Posted on April 05, 2018 at 16:16

Hello Phillipp,

I am notanST employee, however, the reply I linked you to was written by

Batek.Miroslav

‌, who is an ST employee, so I would consider this official.

Best Regards,

David

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.