2023-08-08 1:43 AM
I'm using the LSM6DSOX which can measure ±2000dps and ±16g for each axis with the correct settings. I'm wondering if there is a reliable way to detect if the motion of the sensor went beyond those limits during a given time window. Does the sensor reliably return the maximum/minimum 16bit integer value? Is there some other trick?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.