MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM6DSO32 ultra low power mode not working

Hello,I am using a LSM6DSO32 on a custom board.  As an attempt to save power in sleep mode we want to place the device in ULP (ultra low power mode) as specified by the datasheet.  I have attached my function that initializes the device in ULP mode a...

SDZELL18 by Associate II
  • 3459 Views
  • 4 replies
  • 1 kudos

STEVAL-STWINKT1B is not connecting to wifi

Hello. I made all the adjustments for my STEVAL kit. I also installed the necessary binary file in the Wifi module (Dsh predmnt). According to the guide I gave in the link, I stay on page 12 step 8. When I enter the wifi id password, it does not conn...

bcryhun by Associate II
  • 2310 Views
  • 3 replies
  • 0 kudos

Resolved! LSM6DSL Linux driver, Temperature reading not implemented

Hi Everyone, Below Linux driver for LSM6DSL device has no method to read the temperature sensor. https://elixir.bootlin.com/linux/latest/source/drivers/iio/imu/st_lsm6dsxIs there a complete Linux driver which reads the temperature as well?thanks,   

RAlma.1 by Associate III
  • 3245 Views
  • 4 replies
  • 2 kudos

LPS28DFW bias stability / difference with other LPS28DFW

Hi,I have two LPS28DFW in my application. The absolute value as well as the difference is important here. I noticed that there is a difference of around 30 Pa. Is it reasonable to assume that this difference is roughly constant in the future? I teste...

LSM6DSV16X drift issue

Hi!We are a group trying to get reliable rotation data out of the LSM6DSV16X sensor. The accumulated error values in the datasheet seemed promising. However, we are currently in a state, where the sensor is returning gyroscope data, but the actual ob...

Gorbit99 by Associate III
  • 4829 Views
  • 5 replies
  • 2 kudos

ISM330DLC, no accelerometer or gyroscope data in FIFO

Greetings,I have been trying to read the sensors from the ISM330DLC using its FIFO. However, when reading the number of samples (FIFO_STATUS1/2), it remains 0 with just dataset 1 and 2 enabled. When enabling dataset 4 with either, or and temperature ...

Asm330 low frequency behavior

Hi I have a questionI am using asm330lhh gyroscopeThe sensor is great but I see some kind of low frequency behavior in the data from this sensorMy ODR is 6667 range is 500The accuracy is good, but this low frequency behavior will eventually cause pro...

image_20230804_231800a997c2ca-dcd2-4cf8-aac5-0027bd9d4e55.jpg image_20230804_231805a044cff2-b268-48bb-a6d7-c22c7c3f092e.jpg
AHass.5 by Associate II
  • 2221 Views
  • 3 replies
  • 0 kudos

ASM330LHB-Query

 Dear team,I'm using ASM330LHB for Electronics Brake control project.Please clarify my queries to use this ASIC in our application.How the ASIC is claimed as ASIL-B? Is there any redundancy in the ASIC itself?How the error detection and error reactio...

ganand05 by Associate
  • 1809 Views
  • 2 replies
  • 0 kudos

pdm2pcm, pcm data noisy , pdm mic nucleo f413zh

hello tout le monde, im worknig on audio project im trying to get data from a pdm microphone as pcm 8 bit and transmit the data via uart  as binary but when i transfer the data from binary to audio via audacity i can hear just noise nothing else, als...

zohbou1 by Associate
  • 2354 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.