2021-07-15 1:25 AM
Solved! Go to Solution.
2021-07-15 1:26 AM
The MLC is running completely on ISM330DHCX. The only thing needed from the host microcontroller is to program the sensor at every power cycle since the sensor it is not provided with a programmable flash memory. If the host microcontroller can program the sensor with sequential writes via IF (i2c, SPI, etc...), host FW is not playing any role with MLC.
2021-07-15 1:26 AM
The MLC is running completely on ISM330DHCX. The only thing needed from the host microcontroller is to program the sensor at every power cycle since the sensor it is not provided with a programmable flash memory. If the host microcontroller can program the sensor with sequential writes via IF (i2c, SPI, etc...), host FW is not playing any role with MLC.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.