2019-10-25 3:59 PM
All of the examples of usage that I have seen for the LSM6DSL have been with the STM32 Cortex-M3 and -M4 microcontrollers. I assume that is due to the library calculations that must be made in the support library for this accelerometer/gyro.
Is it possible to use the LSM6DSL as just a simple wake-up interrupt for a Cortex-M0 (STM32L0) controller? I don't need to know, for example, whether a person is standing or walking or running; I just need to know they've moved (within some reasonable tolerance).
2019-10-25 6:14 PM
These are SPI xor I2C devices with little computation on top.
8 bit MCUs like STM8 have even compiler provided math float libraries.
So, technically, it would only be a matter of latency time.
2019-10-28 8:22 AM
I am not even looking at doing any calculation with the data. Rather, I am simply looking for a way to wake the MCU based on the wake-up interrupt from the LSM6DSL.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.