2014-06-18 5:24 AM
Hi guys,
I have jsut started using the Inemo_m1 discovery board.
After Installing the software and doing some hello world projects (using KEIL IDE;debugged via ST-Link debugger), I decided to setup communication with the on board accelerometer.
In the installation directory: STEVAL-MKI121V1\Discovery-M1_Fw_Package\iNemo_M1_Applications\Source\examples
There is a source file named: LSM303DLHC_AccDataReady.c
I created a project, set the code in this .c file as the main function and compiled the project. After including some source and header files, the project compiled succesfully.
I loaded the project onto the inemo and started debugging with the ST-Link debugger.. The debugger jams atinstruction ' while(!xAccDataReady);' waiting for the accelerometer data ready interrupt to happen.
I have gone through all the code and it seems that all has been well set, I really can't figure out what is wrong... anybody had any try to this code? Any help is much appreciated..
regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.