2021-04-28 3:31 AM
Hello,
for a new project we are avalutaing the use of an iNEMO inertial module in conjunction with the motion fx library with the goal of doing position estimation with dead reckoning.
My doubt is about the library, since we are forced to use a thrid party MCU (an ARM M4), can I import the library on any ARM M0/M4/M7 mcu? Or does it target ONLY st devices?
Thank you,
Davide
2021-04-28 5:41 AM
Hi Davide @Davide G_Oiovanelli ,
it is possible to port -in general- the X-CUBE-MEMS1 libraries on MUCs other than STM32 ones, but always based on ARM Cortex architecture.
However, it cannot be done directly from the customer, unfortunately: the library, in this case the MotionFX one, must be specifically compiled from ST support under the signature of License Agreement (LUA).
You have to contact the OLS at this link or a Sales offices and representatives office from your region at this other link.
Let me know if you can get a feedback from them.
-Eleon
2021-04-28 5:45 AM
Hi Eleon,
thank you. I'll forward the information to my supervisor that will contact the OLS or the Sales offices.
In case I have other problems I'll post them here, thank you again.
Davide.
2021-05-24 11:43 PM
Hi Eleon,
I contacted the ST support to ask for having the library compiled for a third party MCU, however I get a negative response from them (they say the library is only for STM32s).
If you don't have any other suggestion I would say that the library cannot be run on other vendors' mcu.
Davide.
2025-01-07 5:41 AM
Hi,
I had also requested for the same. I am using a NXP controller. I am getting two different answers from ST. One guy is saying it is portable and another saying it is only for ST. I also got the MotionFX library for my nxp controller, but when integrating i am getting Hard fault error.
Regards,
Tarun
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.