cancel
Showing results for 
Search instead for 
Did you mean: 

In ISM330DHCX the MLC can run up to 104Hz, that means that we cannot detect any abnormal frequency above 52 Hz? Why is the MLC limited to 104Hz if the maximum sensor ODR (Gyro or XL) is 6.67kHz?

Evelina CAMILLERI
ST Employee
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Evelina CAMILLERI
ST Employee

Correct, MLC can run up to 104Hz and thus cannot correctly detect any vibration frequency higher than 52Hz. The MLC elaboration rate is limited to 104Hz due to computational limitations, but ST is working towards the direction of increasing the elaboration rate with the next generation of inertial sensors.

View solution in original post

1 REPLY 1
Evelina CAMILLERI
ST Employee

Correct, MLC can run up to 104Hz and thus cannot correctly detect any vibration frequency higher than 52Hz. The MLC elaboration rate is limited to 104Hz due to computational limitations, but ST is working towards the direction of increasing the elaboration rate with the next generation of inertial sensors.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.