2021-04-06 2:18 AM
2021-04-07 7:20 AM
Hi @Bbile.1 ,
I'm not an expert of this tool, so I added the LoRa topic for more help.c
Checking the I-CUBE-LRWAN firmware function pack (2.0.0 version), I can see that the drivers for the sensors can be found in the \Drivers\BSP\Components.
Then, in the UM2073 user manual at p. 38 there is the End_node application description that might be of your interest: the specific project can be found in the \Projects\B-L072Z-LRWAN1\Applications\LoRaWAN\LoRaWAN_End_Node\EWARM, and the file dedicated to the sensors' configuration should be the sys_sensor.c.
Please note also that you need the X-NUCLEO-IKS01A2 or the X-NUCLEO-IKS01A3 board for sensors' connection.
-Eleon
2021-04-07 8:34 AM
Yeah, I don't think the problem here is reach.
The question isn't well stated, and has a random screen shot.
Is it a question of how to drive IAR? Or do static source analysis?
Do you have a supervisor or more senior staff member who can work with you?
Which project specifically within the LRWAN V1.3.1?
On what board or combinations of boards?
Doesn't grep or find-in-files provide some association?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.