2020-09-25 12:52 AM
Hello
I have been trying to setup 6D orientation interrupt using IIS2DLPC and I am not getting any interrupts on INT1 pin when the orientation changes beyond threshold.
For debugging I tried printing SIXD_SRC (3Ah) and ALL_INT_SRC (3Bh) registers. In the SIXD_SRC register I am seeing the bit 6D_IA (a change in position is detected) is set and in register ALL_INT_SRC I am seeing the bit 6D_IA (a change in position detected) is also set but no interrupts are generated.
I have also tried changing Interrupt active high/low and Latched Interrupt settings both didnt work. Also tried adding internal pullup and pulldown from the micro controller that also didn't work.
I2C settings done for 6D orientation interrupt:
1. Write 64h in CTRL1 // Turn on the accl // ODR = 200 Hz, High-Performance
2. Write 04h in CTRL6 // FS ±2 g, LOW_NOISE enabled
3. Write 20h in CTRL7 // Do not use low-pass filter for 6D, enable interrupts
4. Write 40h in TAP_THS_X // Set 6D threshold (6D_THS[1:0] = 10b = 60 degrees)
5. Write 80h in CTRL4_INT1_PAD_CTRL // 6D interrupt driven to INT1 pin
Am I missing something or should I be doing anything extra?
2020-09-25 1:50 AM
Hi @KS.9 ,
you can compare your code with the official C example on Github repository for the IIS2DLPC (in particular, this file: iis2dlpc_orientation.c).
The only difference I can see is that the ODR is configured after the other settings are ready done and that the LPASS_ON6D bit of CTRL7 (3Fh) register has been enabled, so:
3. Write 21h in CTRL7 // Use low-pass filter for 6D, enable interrupts
/*Restore default configuration */
iis2dlpc_reset_set(&dev_ctx, PROPERTY_ENABLE);
do {
iis2dlpc_reset_get(&dev_ctx, &rst);
} while (rst);
/*Set full scale */
iis2dlpc_full_scale_set(&dev_ctx, IIS2DLPC_2g);
/*Configure power mode */
iis2dlpc_power_mode_set(&dev_ctx, IIS2DLPC_CONT_LOW_PWR_LOW_NOISE_12bit);
/*Set threshold to 60 degrees */
iis2dlpc_6d_threshold_set(&dev_ctx, 0x02);
/*LPF2 on 6D function selection. */
iis2dlpc_6d_feed_data_set(&dev_ctx, IIS2DLPC_LPF2_FEED);
/*Enable interrupt generation on 6D INT1 pin. */
iis2dlpc_pin_int1_route_get(&dev_ctx, &int_route.ctrl4_int1_pad_ctrl);
int_route.ctrl4_int1_pad_ctrl.int1_6d = PROPERTY_ENABLE;
iis2dlpc_pin_int1_route_set(&dev_ctx, &int_route.ctrl4_int1_pad_ctrl);
/*Set Output Data Rate */
iis2dlpc_data_rate_set(&dev_ctx, IIS2DLPC_XL_ODR_200Hz);Please check your application with this modified configuration and let me know.
-Eleon
2020-09-25 2:49 AM
Hi @Eleon BORLINI
Thanks for the response.
I tried the orientation example given in the Github repository still I am not getting interrupts.
I have also tried other examples there also I am not getting any interrupts.
2020-09-25 3:46 AM
Hi @KS.9 ,
but are you getting correct acceleriation values when you just read the output registers?
-Eleon
2020-09-25 4:01 AM
Hi @Eleon BORLINI
The acceleration values from the output registers are correct.
Thanks
KS
2020-10-02 2:42 AM
Hi @KS.9 ,
sorry for the delayed feedback... Did you try to run your code with other IIS2DLPC samples?
-Eleon
2024-04-16 6:40 AM
Has this been resolved? I am facing a similar issue, I am not getting any interrupt nor I see anything being set in the SIXD_SRC register as it's always reporting 0. however if I read the Output registers (OUT_Y_LOW, OUT_Y_HIGH, OUT_Z_LOW, OUT_Z_HIGH) I see the correct data and it seems to work fine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.