2016-10-19 1:31 AM
Hello,
I have been playing with the IIS2DH configuration and there are couple of settings that are not clear for me, for example: - what is the I1_DRDY2 used for? - similarly I'm not sure about I1_AOI1 vs I1_AOI2 interrupt functionality - in CTRL_REG6, as per spec I2_INT1 and I2_INT2 redirect interrupt functions 1 and 2 respetively onto INT2 pin, but what is the actual difference between function 1 and funtion 2? It would be great if someone could clarify it. Thanks. #iis2dh #drdy1 #drdy2 #aoi22016-10-21 7:35 AM
The IIS2DH has two configurable interrupt generators, first one is configured by registers 30h-33h and the second one by registers 34h-37h. The generators can be linked to INT1 and/or INT2 pins. Bits I1_AOI1 and I1_AOI2 in register CTRL_REG3 (22h) select the generators for pin INT1, similarly bits I2_INT1 a I2_INT2 in register CTRL_REG6 (25h) select the generators for pin INT2.
I1_DRDY2 in CTRL_REG3 (22h) concerns a feature that is not available in this device, basically it is a mistake in the datasheet.
Best regards
Miroslav
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.