2022-03-02 3:00 PM
I am writing a driver to retrieve data from the I3G4250D gyroscope embedded in the STM32F411VE discovery board (MB1115D). When the sensor starts up, the first 1 second of data contains an invalid temperature value (typically showing -7). After one second this value changes and is accurate from then on.
I noticed from the datasheet that there is a 1 Hz refresh rate for the temperature, which makes sense given what I'm seeing. I'm wondering if there's a way I can retrieve valid temperature data earlier than 1 second, i.e. if I can delay when this refresh rate begins. This temperature data is critical for our calibration calculations, so having bad data is messing up our algorithms.
Solved! Go to Solution.
2022-03-04 7:35 AM
Hi @AWool.1 , you are right, the I3G4250D temperature sensor refresh rate is 1Hz, so you have to wait at least 1 second to get a correct readout of the temperature data. Unfortunately I don't believe there is a way to overcome this limitation, maybe you can try to read at least 1 second after the power up.
/tim
2022-03-04 7:35 AM
Hi @AWool.1 , you are right, the I3G4250D temperature sensor refresh rate is 1Hz, so you have to wait at least 1 second to get a correct readout of the temperature data. Unfortunately I don't believe there is a way to overcome this limitation, maybe you can try to read at least 1 second after the power up.
/tim
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.