2023-05-28 9:37 AM
Im testing the entry mode and i try the vibration app. I think my accelerometer dosent work because the led is always on (everytime detected a event), how can i check it?
2023-05-28 11:24 PM
Actually i have the same problem with the microphone, i was testing the cry detection app, and was the same, everytime detected the event, so i dont know if i need to put a treshold or something.
2023-05-29 6:20 AM
Hi @Sergio Abbattista Hernández ,
If you are using the default firmware, please try to load the sensor fusion and let me know if the accelerometer works. Otherwise, you can try the function pack FP-SNS-ALLMEMS2 available on our website.
2023-05-29 7:01 AM
Yeah, the sensor fusion but i dont know why the Vibration monitor is not working, everytime detected a event.
2023-05-30 5:18 AM
So can you confirm me that the sensor fusion works?
If the problem is now the vibration monitoring, can you check if you have the .csv file (gold_vibration_pattern) for the comparison in the SD Card?
2023-05-31 1:03 PM
1) Verify hardware connections and ensure everything is properly connected. 2) Review the code for correct configuration. 3) Test with different apps or examples to determine if the issue is with your code. 4) Ensure sufficient power, and up-to-date firmware.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.