2020-01-07 3:20 AM
I am looking to make audio circuit. I need suggestion for microphone followed by noise cancellation ICs.
Any help will be appreciated.
Thanks
Sudhanshu.
2020-01-23 9:28 AM
Hi @SMeht.1 , as I wrote before, the reference design for an active noise cancelling and, better, beam-forming app is the Bluecoin tool, aka STEVAL-BCNKT01V1 (the first one you mentioned in the comment here above). The other suggested evaluation tool is the X-NUCLEO-CCA02M2. Both them can be interfaced with the tool you suggested, the NUCLEO-F410RB, that acts as master board. You can find the FW libraries for the PDM to I2S conversion in the Middlewares folder of the function pack FP-AUD-SMARTMIC1.
I suggest you not to use the STEVAL-MKI126V3 / STEVAL-MKI138V1 and related SW, because they are nrnd products and are no more supported.
2020-02-27 5:13 AM
Hello @Eleon BORLINI
Thanks for your reply.
As per your suggestion, i have started doing POC with STEVAL-BCNKT01V1 .
it works fine when i record sound on PC using USB.
My next action is to make it compatible with product. I want to take this audio over I2S and send this to bluegiga wt32i iwrap6 module.
I am getting challange in this.
i want to reduce following items of STEVAL-BCNKT01V1 module.
LRCLK (Word Select Clock) - 8.00 kHz
BCLK (Bit Clock) - 385 kHz
I can compile code. Can you suggest how to lower this. I am using STM32CubeFunctionPack_SMARTMIC1_V2.0.0.
other wise voice on other side of Bluegiga module is cracking.
Thanks
Sudhanshu Mehta
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.