2020-11-22 3:56 AM
There are a lot Sensors but lsm9ds1 is not listed!
regards
2020-11-23 1:35 AM
Hi @Jörg Boge ,
do you refer to the fact that, for example, in the X-CUBE-MEMS1 firmware function pack there are no LSM9DS1 drivers in the Drivers\BSP\Components folder?
If so, my suggestion is to consider the LSM9DS1 C drivers and examples on Github and insert them in your CubeMX project, configuring it according to the hardware platform you are using (especially for the correct configuration of the SPI communication interface).
Please let me know if this can be useful for your purposes.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.